TMS320C6000 Highest Performance DSP Platform | ||
> Platform Summary | C64x DSP Benchmarks Filters Vector FFTs Search Math Imaging Telecom |
Benchmark | Description | Formula |
---|---|---|
General FIR | Implements a general purpose 16-bit FIR filter. Requires at least 5 filter taps and generates a minimum of one output sample. | cycles = (8 + nh') * nr'/4 + 19 For nh = 32 and nr = 100, cycles = 1100. |
Horizontal Scaling | Scales a set of 'in_len' samples to a set of 'out_len' samples using a polyphase filter bank. The number of filters is given by 'n_hh' and the length of the filters is given by 'l_hh'. The scale factor is given by ratio 'out_len / in_len'. | cycles = 0.5 * out_len * l_hh * (1+k) + 30. If (l_hh % 8) == 0 then k = 1/(4*l_hh) else k = 0. For l_hh = 16, in_len = 1024, and out_len = 1366, cycles = 11129. For l_hh = 8, in_len = 640, and out_len = 120, cycles = 525. |
Vertical Scaling | Calculates a single row of output from multiple rows of input for the vertical pass of a scaling filter, using a polyphase filter bank. Each row of input and output is 'cols' pixels long. The polyphase filter bank contains 'n_hh' filters that are 'l_hh' taps long. | cycles = (0.33 * l_hh * cols) + 6 * l_hh + 32 For cols = 800 and l_hh = 4, cycles = 1056. |
Benchmark | Description | Formula |
---|---|---|
Dot Product | Performs the dot product of two arrays by multiplying the individual elements of two arrays and summing them up to return the result. | cycles = count/4 + 16 For count = 720, cycles = 196 |
Benchmark | Description | Formula |
---|---|---|
Complex Radix 4 FFT | Performs a Complex Radix 4 FFT over N points. N must be a power of 4. | cycles = 1.25*nsamp*log4(nsamp) - 0.5*nsamp + 23*log4(nsamp) - 1. For N = 64, cycles = 276. For N = 256, cycles = 1243. For N = 1024, cycles = 6002. |
Benchmark | Description | Formula |
---|---|---|
3x3 Correlation | Performs the 3x3 Correlation of an input image with a 3x3 mask, that is typically part of the image. Correlation sum is rounded and shifted to produce an eight bit result. | cycles = (cols - 2) * 1.25 + 20 For cols = 720, cycles = 925. |
8x8 Block Motion Estimation | Locates the position in a reference image which most closely matches an 8x8 block from a source image, using the Minimum Absolute Difference metric. Searches over a range that is 'H' pixels wide and 'V' pixels tall within a reference image that is 'pitch' pixels wide. | cycles = H * V * 8 + 54 For H = 64 and V = 32, cycles = 16438. |
3x3 Median Filter | Performs a 3x3 median filter operation for a row of image data. Each output point is the median value selected from the 9 points under the filter kernel. | cycles = cols * 2 + 32 For cols = 256, cycles = 544 |
Horizontal Wavelet | Performs a 1D Periodic Orthogonal Wavelet decomposition. An input signal x[n] is low pass and high pass filtered and decimated by two to produce a reference signal r1[n] and d[n] respectively. | cycles = (cols * 2) + 25 For cols = 256, cycles = 537. For cols = 512, cycles = 1049. |
Vertical Wavelet | Performs the vertical pass of 2D wavelet transform, on 8 rows to produce two lines worth of output, one being the low-pass and the other being the high pass result. Each row of input and output is of length 'cols'. | cycles = 4*cols + 96 For cols = 256, cycles = 1120. For cols = 512, cycles = 2144. |
8x8 Block IDCT, IEEE-1180 Compliant. | Performs an 2-D Inverse Discrete Cosine Transform on 'num_idcts' 8x8 blocks. Input data is expected in 12Q4 format. | cycles = 62 + 92 * num_idcts For num_idcts = 6, cycles = 614. For num_idcts = 24, cycles = 2270. |
Quantize | Quantizes blocks of values by multiplying their contents with a second blocks of values that contains reciprocals of the quantization terms. This step corresponds to the quantization that is performed in 2-D DCT-based compression techniques. | cycles = 26 + (blk_size/16) * num_blks * 8 For blk_size = 64 and num_blks = 6, cycles = 218. For blk_size = 256 and num_blks = 24, cycles = 3098. |
Benchmark | Description | Formula |
---|---|---|
Viterbi GSM | Performs the Viterbi Decode for Full-Rate GSM, including traceback. | cycles = 14 * n + 33 For n = 189, cycles = 1377. |
REED SOLOMON: Syndrome Accumulate | Calculates the syndrome values for the received codeword array. These are used to detect errors in the incoming data. This is the first stage of the Reed Solomon decoder. | cycles = (T/4)*N + 32 |
REED SOLOMON: Berlekamp Massey | Solves the error locator polynomial equation, Lambda * S = 0, using the Berlekamp-Massey algorithm. (The * denotes convolution.) | cycles = 30*T + 6 |
REED SOLOMON: Chien Search | Uses the Chien Search algorithm to locate the zeros for an error polynomial in a Reed-Solomon decoder. | cycles = 263 (for GF256) |
REED SOLOMON: Forney | Corrects errors in the received codeword array in-place. It uses the inputs generated by Syndrome Accumulate, Berlekamp-Massey, and Chien Search to perform the correction. | cycles = 12*T + 50 |