SBAS661C February 2015 – May 2021 ADS1262 , ADS1263
PRODUCTION DATA
Reset the ADC by using the reset command (opcode = 06h or 07h). Toggle CS high first to make sure the serial interface resets before sending the command. For applications that tie CS low, see the Section 9.4.4.5 section for information on how to reset the serial interface. After sending the reset command, provide an 8-fCLK-cycle delay before sending the next command, as shown in Figure 9-54 and Table 9-32.
PARAMETER | MIN | UNIT(1) | |
---|---|---|---|
th(CMCM) | RESET command to next command: hold time | 8 | tCLK |