SBASAK4B March 2023 – April 2024 ADS127L21
PRODUCTION DATA
FIR3 coefficients are available without the need to supply custom coefficients. The default coefficients are selected by the FLTR_SEL[2:0] bits = 000b of the FILTER1 register. The default coefficients feature linear phase response, low pass-band ripple, narrow transition band, and high stop-band attenuation.
Figure 7-14 through Figure 7-18 illustrate the default wideband filter frequency response. Figure 7-14 shows the pass-band ripple. Figure 7-15 shows the frequency response at the transition band.
Figure 7-16 illustrates the filter response up to fDATA for OSR ≥ 64. The stop band begins at fDATA / 2 to reduce signal aliasing. Figure 7-17 illustrates the filter to fMOD. In the stop-band region, signal frequencies intermodulate with multiples of the chop frequency at fMOD / 32. Thus, creating a series of response peaks that exceed the attenuation provided by the digital filter. The width of the response peaks is twice the filter bandwidth. Stop-band attenuation is improved when the ADC input is filtered by an analog antialias filter. See the Typical ApplicationsA-Weighting Filter DesignTHS4551 Antialias Filter Design section for details of a fourth-order antialias filter at the ADC input.
OSR ≥ 64 |
OSR = 32 |
Figure 7-18 shows the filter response at fMOD. As shown, the filter response repeats for input signals at fMOD. If not removed by an antialias filter, signal frequencies at fMOD appear as aliased frequencies in the pass band.
Aliasing also occurs with input frequencies occurring at multiples of fMOD. These frequency bands are defined by:
where:
The group delay of the filter is the propagation time for an input signal to appear at the output of the filter. Because the filter is a linear-phase design, the envelope of a complex input signal is undistorted by the filter. The group delay (expressed in units of time) is constant versus frequency, equal to 34 / fDATA. After a step input is applied, fully settled data occur 68 data periods later. Figure 7-19 illustrates the filter group delay (34 / fDATA) and the settling time to a step input (68 / fDATA).
The digital filter is restarted when the ADC is synchronized. The ADC suppresses the first 68 conversion periods until the filter is fully settled. There is no need to discard data after synchronization. The time of data suppression is the conversion latency time as listed in the latency time column of Table 7-12. Sixteen fCLK cycles of overhead time are incurred for all data rates. If a step input is applied randomly to the conversion period without synchronizing, the next 69 conversions are unsettled data. The –0.1dB frequency of the amplitude response is 0.4125 × fDATA and the –3dB frequency is 0.4374 × fDATA for all data rates.
MODE | fCLK (MHz) |
OSR | DATA RATE (kSPS) |
–0.1dB FREQUENCY (kHz) |
–3dB FREQUENCY (kHz) |
LATENCY TIME(3)
(µs) |
---|---|---|---|---|---|---|
Max speed | 32.768 | 32 | 512 | 211.2 | 223.9 | 135.5 |
High speed | 25.6 | 400 | 165 | 174.96 | 173.4 | |
Mid speed | 12.8 | 200 | 82.5 | 87.48 | 346.9 | |
Low speed | 3.2 | 50 | 20.63 | 21.87 | 1387.8 | |
Max speed | 32.768 | 64 | 256 | 105.6 | 112.0 | 270.4 |
High speed | 25.6 | 200 | 82.5 | 87.48 | 346.1 | |
Mid speed | 12.8 | 100 | 41.25 | 43.74 | 692.2 | |
Low speed | 3.2 | 25 | 10.31 | 10.94 | 2768.7 | |
Max speed | 32.768 | 128 | 128 | 52.8 | 55.99 | 540.0 |
High speed | 25.6 | 100 | 41.25 | 43.74 | 691.2 | |
Mid speed | 12.8 | 50 | 20.63 | 21.87 | 1382.3 | |
Low speed | 3.2 | 12.5 | 5.1562 | 5.468 | 5529.2 | |
Max speed | 32.768 | 256 | 64 | 26.4 | 28.00 | 1079.2 |
High speed | 25.6 | 50 | 20.625 | 21.87 | 1381.3 | |
Mid speed | 12.8 | 25 | 10.31 | 10.93 | 2762.6 | |
Low speed | 3.2 | 6.25 | 2.578 | 2.734 | 11051 | |
Max speed | 32.768 | 512 | 32 | 13.2 | 14.00 | 2157.6 |
High speed | 25.6 | 25 | 10.312 | 10.935 | 2761.6 | |
Mid speed | 12.8 | 12.5 | 5.156 | 5.467 | 5523.3 | |
Low speed | 3.2 | 3.125 | 1.289 | 1.367 | 22093 | |
Max speed | 32.768 | 1024 | 16 | 6.6 | 7.998 | 4314.2 |
High speed | 25.6 | 12.5 | 5.156 | 5.467 | 5522.3 | |
Mid speed | 12.8 | 6.25 | 2.578 | 2.734 | 11045 | |
Low speed | 3.2 | 1.5625 | 0.645 | 0.6834 | 44178 | |
Max speed | 32.768 | 2048 | 8 | 3.3 | 3.499 | 8627.8 |
High speed | 25.6 | 6.25 | 2.578 | 2.734 | 11044 | |
Mid speed | 12.8 | 3.125 | 1.289 | 1.367 | 22087 | |
Low speed | 3.2 | 0.78125 | 0.322 | 0.3417 | 88348 | |
Max speed | 32.768 | 4096 | 4 | 1.65 | 1.750 | 17254 |
High speed | 25.6 | 3.125 | 1.289 | 1.367 | 22086 | |
Mid speed | 12.8 | 1.5625 | 0.645 | 0.6834 | 44172 | |
Low speed | 3.2 | 0.390625 | 0.161 | 0.1709 | 176690 |