SBASA22A september 2022 – july 2023 ADS131B26-Q1
PRODUCTION DATA
The RESET command resets the device and sets all user registers to the respective default values. The command is latched by the device at the last SCLK falling edge of the output CRC word. Terminating the frame before the output CRC word is shifted out on SDO causes the RESET command to be ignored. A reset occurs immediately after the command is latched. The DRDYn pin transitions low at the same instance. The host must wait for tREGACQ after reset or for the DRDYn rising edge to make sure the device completes the reset process before communicating with the device.
The RESETn status bit and the command response in the next frame indicate if the RESET command executed successfully or if an error occurred that prevented the RESET command from executing. A NULL command is executed if the RESET command did not execute.
Figure 8-32 shows a RESET command frame where no faults occurred during the communication.