Powering the PA on and off in a controlled routine
is necessary to prevent the VGS voltage from being too high when the
VDRAIN is applied. Such a state causes the PA to operate in
saturation mode which can result in thermal damage in the PA or any connected board.
Powering on a PA requires the following steps:
- First, apply the VGS signal to the PA. The VGS voltage
must transition to the VGS pinch-off voltage or lower. This makes
sure that when the VDRAIN voltage is applied, the gate is already
low.
- Next, enable the drain voltage supply and allow the VDRAIN to be powered to the nominal value (50 V, for example). As the VGS is at the pinch-off voltage, IDS must be minimal.
- After the VDRAIN is applied, increase the VGS bias voltage to set the desired power output of the PA.
- Finally, enable the RF signal. This allows the PA to transmit a signal.
The PA can be safely shut down by reversing the power-on steps.
- Disable the RF signal from the PA.
- Reduce the VGS voltage to the pinch-off value, eliminating the power output of the PA.
- Disable the VDRAIN voltage by sending a disable signal to the drain supply.
- Finally, the VGS voltage can be allowed to collapse to ground as the PA is fully disabled.