In this mode, all ADC digital samples are
accumulated and averaged after every 50 µs. At each rising edge of the ADC reset
signal, one averaged ADC conversion value is written into the output registers
sequentially, as follows (see Figure 8-29):
- At the 25% reset signal, the
first averaged ADC sample is written to register 2Ah (Decimal address =
42).
- At the 50% reset signal, the
second averaged ADC sample is written to register 2Bh (Decimal address =
43).
- At the 75% reset signal, the
third averaged ADC sample is written to register 2Ch (Decimal address =
44).
- At the next 0% reset signal,
the fourth averaged ADC sample is written to register 2Dh (Decimal address =
45).
- Every time the registers 2Ah and 2Bh are updated, the contents of the
difference register 2Eh is updated. Similarly, every time the registers 2Ch
and 2Dh are updated, the contents of the difference register 2Fh is
updated.
The number of samples to be used per
conversion phase is specified in the CONTROL1 register (NUMAV[7:0]). The user must
specify the correct value for the number of averages, as described in Equation 6:
Equation 6. ![GUID-BCE22DDB-9BE7-4BAD-8387-761B82E00F10-low.gif](/ods/images/SBAS650C/GUID-BCE22DDB-9BE7-4BAD-8387-761B82E00F10-low.gif)
Note that the 50-µs factor corresponds to a case where the internal clock of the AFE (after division) is exactly equal to 4 MHz. The factor scales linearly with the clock period being used.
Note that the number of average conversions is limited by 25% of the PRF. For example, eight samples can be averaged with PRF = 625 Hz, and four samples can be averaged with PRF = 1250 Hz.
Note: Every time Register 2Ah or Register
2Bh are updated, the difference (Register 2Ah - register 2Bh) is written into
register 2Eh. Every time Register 2Ch or Register 2Dh are updated, the difference
(Register 2Ch - register 2Dh) is written into register 2Fh.
Note: Every time Register 2Ah or Register
2Bh are updated, the difference (Register 2Ah - register 2Bh) is written into
register 2Eh. Every time Register 2Ch or Register 2Dh are updated, the difference
(Register 2Ch - register 2Dh) is written into register 2Fh.