SLASEU7 March 2023 AFE781H1 , AFE881H1
PRODUCTION DATA
Figure 7-1 shows that the resistor string structure consists of a series of resistors, each of value R. The code loaded to the DAC determines the node on the string at which the voltage is tapped off to be fed into the output amplifier. The voltage is tapped off by closing one of the switches connecting the string to the amplifier. The resistor string architecture has inherent monotonicity, voltage output, and low glitch.