SBASA35B June 2020 – September 2024 AMC3330-Q1
PRODUCTION DATA
Figure 7-6 shows a layout recommendation with the critical placement of the decoupling capacitors. The same component reference designators are used as in the Power Supply Recommendations section. Decoupling capacitors are placed as close as possible to the AMC3330-Q1 supply pins. For best performance, place the sense resistor close to the INP and INN inputs of the AMC3330-Q1 and keep the layout of both connections symmetrical.
This layout is used on the AMC3330-Q1 EVM and supports CISPR-25 compliant electromagnetic radiation levels.