SLUSE99C September 2021 – January 2023 BQ25180
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
When a valid input source is connected (VIN > VUVLO and VBAT+VSLEEPZ ≤ VIN < VIN_OVP), the state of the CHARGE_DISABLE bit and the TSMR pin determines whether a charge cycle is initiated. When the CHARGE_DISABLE bit is set to disable charging, VHOT < VTS < VCOLD and a valid input source is connected, the battery discharge FET is turned off, preventing any charging of the battery. Note that supplement behavior is independent of the CHARGE_DISABLE bit.
The following figure illustrates a typical charge cycle.