SLUSE97 November 2023 BQ76905
PRODUCTION DATA
PIN | I/O | TYPE | DESCRIPTION | |
---|---|---|---|---|
NO. | NAME | |||
1 | VC3A | I | IA | Sense voltage input pin for the negative terminal of the fourth cell from the bottom of the stack, and return balance current for the fourth cell from the bottom of the stack |
2 | VC3B | I | IA | Sense voltage input pin for the third cell from the bottom of the stack, and balance current input for the third cell from the bottom of the stack. |
1 | VC2 | I | IA | Sense voltage input pin for the second cell from the bottom of the stack, balance current input for the second cell from the bottom of the stack, and return balance current for the third cell from the bottom of the stack |
2 | VC1 | I | IA | Sense voltage input pin for the first cell from the bottom of the stack, balance current input for the first cell from the bottom of the stack, and return balance current for the second cell from the bottom of the stack |
3 | VC0 | I | IA | Sense voltage input pin for the negative terminal of the first cell from the bottom of the stack, and return balance current for the first cell from the bottom of the stack |
6 | SRP | I | IA | Analog input pin connected to the internal coulomb counter peripheral for integrating a small voltage between SRP and SRN, where SRP is the top of the sense resistor. A charging current generates a positive voltage at SRP relative to SRN. |
7 | SRN | I | IA | Analog input pin connected to the internal coulomb counter peripheral for integrating a small voltage between SRP and SRN, where SRN is the bottom of the sense resistor. A charging current generates a positive voltage at SRP relative to SRN. |
8 | TS | I/O | I/OA | Thermistor or general-purpose ADC input and functions as wakeup from SHUTDOWN |
9 | DSG | O | OA | NMOS Discharge FET drive output pin |
10 | CHG | O | OA | NMOS Charge FET drive output pin |
11 | VSS | — | P | Device ground |
12 | SCL | I/O | I/OD | I2C serial communication bus clock |
13 | SDA | I/O | I/OD | I2C serial communication bus data |
14 | ALERT | O | OD | Digital interrupt output pin |
15 | REGOUT | O | OA | LDO output, which can be programmed for 1.8 V, 2.5 V, 3.0 V, 3.3 V, or 5.0 V |
16 | REGSRC | I | IA | Input pin for REGOUT LDO, also functions as supply for the CHG and DSG FET drivers |
17 | BAT | I | P | Primary power supply input pin |
18 | VC5 | I | IA | Sense voltage input pin for the fifth cell from the bottom of the stack, balance current input for the fifth cell from the bottom of the stack, and the top-of-stack measurement point |
19 | VC4A | I | IA | Sense voltage input pin for negative terminal of the fifth cell from the bottom of the stack, and return balance current for the fifth cell from the bottom of the stack |
20 | VC4B | I | IA | Sense voltage input pin for the fourth cell from the bottom of the stack, and balance current input for the fourth cell from the bottom of the stack |