SBOS998C June 2021 – March 2022 BUF802
PRODUCTION DATA
The BUF802 is intended to operate with supplies ranging from ±4.5 V to ±6.5 V. The BUF802 can operate on either single-sided supplies or split supplies. When using split supplies, the supplies may be symmetrically balanced around GND or asymmetric. For best AC performance, the input and output signal should be centered around the mid-supply.
Minimize the distance between the power-supply pins and decoupling capacitors. The high frequency capacitors (< 0.1 µF) should be placed close to the supply-pins on the same side of the PCB as the BUF802. Larger capacitors (> 1 µF) can be placed further away from the device. Section 11 has additional details on decoupling capacitor layout and routing.
The BUF802 has two sets of supply pins: VS+ and VS-; VSO+ and VSO-. The separation of the input and output stage supply pins minimize spurious cross-talk and maximizes transient decoupling between the two stages. Figure 8-1 shows how both sets of supply pins are internally connected through back-to-back diodes. It is therefore imperative that the supply pins for the input and output stages are connected to the same potential. As shown in Section 11, maintain separate and individual decoupling capacitors for all the supply pins.