SBAS528D June 2013 – December 2021 DAC7760 , DAC8760
PRODUCTION DATA
The current output stage consists of a
preconditioner and a current source as
conceptualized in Figure 8-3. This stage provides a current output according
to the DAC code. The output range can be
programmed as 0 mA to
20 mA, 0 mA to 24 mA, or 4 mA to 20 mA. An
external boost transistor can be used to reduce
the power dissipation of the device. The maximum
compliance voltage on pin IOUT equals (AVDD – 2
V). In single power-supply mode, the maximum AVDD
is 36 V, and the maximum compliance voltage is 34
V. After power on, the IOUT pin is in a Hi-Z
state.
Resistor RSET (used to convert the DAC voltage to current) determines the stability of the output current over temperature. If desired, an external, low-drift, precision 15-kΩ resistor can be connected to the ISET-R pin and used instead of the internal RSET resistor.
For a 5-V reference, the output can be expressed as shown in Equation 3 through Equation 5.
For a 0-mA to 20-mA output range:
For a 0-mA to 24-mA output range:
For a 4-mA to 20-mA output range:
where
The current-output range is normally set according to the value of the RANGE bits in the Control Register. When both the voltage and current outputs are enabled in dual-output mode, the range is set by the IOUT RANGE bits in the Configuration Register. See Section 8.4.1 for more details. For more details on controlling the current output when both the VOUT and IOUT pins are simultaneously enabled, see Section 9.1.1.