DLPS240A June 2024 – August 2024 DLPA3085
PRODUCTION DATA
The DLPA3085 can be supplied with an adapter. The DLPA3085 uses several warning and detection levels to prevent system damage when the supply voltage is below the predefined level or an interruption occurs.
For example, interruption of the supply voltage occurs when the adapter is switched to another main outlet. A change of supply voltage from 20V to 8V, and thus the OVP level (which is ratio metric, see Section 6.3.2.5.2) could become lower than VLED. An OVP fault is triggered and the system switches off.
The ILLUM_LED_AUTO_OFF_EN (0x01, bit 2) function can be used to prevent the system from turning off in these circumstances. This function disables the LEDs when the supply voltage drops below LED auto-off level. When the ILLUM_LED_AUTO_OFF_EN (0x01, bit 2) function is enabled, once a supply voltage drop is detected to below LED auto-off level, the LEDs switch off and the system starts sending lower current levels to have a lower VLED. After start using lower currents, the LEDs can be switched on again by disabling ILLUM_LED_AUTO_OFF_EN (0x01, bit 2) function. As a result the system can continue working at the lower supply voltage using a lower intensity. Once the mains adapter is plugged in again, the ILLUM_LED_AUTO_OFF_EN (0x01, bit 2) function can be enabled again. The LED currents can be restored to their original levels.