DLPS024G August 2012 – February 2020 DLPC410
PRODUCTION DATA.
If there is a problem with the image displayed, one of the first places to check is the data being presented to the DLPC410. This data is generated by customer application hardware/software and is then presented to the inputs of the DLPC410. If the data is formatted incorrectly or the control information is incorrect, the DLPC410 may not properly receive the data. Please see Row Addressing for a description of how to send data to the DLPC410.