In LOAD2 mode, automatic increment mode and
row address mode can still be used as before, but the largest addressable row is (VRes ÷
2) – 1, where VRes = the vertical resolution of the DMD. The addressable vertical
resolution is reduced by two, although the physical resolution is unchanged. Automatic
increment address mode automatically increments the row address input by one (or
decrement by one for N/S flip). The row address input is remapped, as shown in
Table 6-1 below:
Table 6-1 LOAD2 Row Address
Mapping
ROW ADDRESS
INPUT |
PHYSICAL ROWS
LOADED ON DMD |
0 |
0, 1 |
1 |
2, 3 |
2 |
4, 5 |
3 |
6, 7 |
N |
2N, 2N + 1 |
(VRes ÷ 2) –
1 |
VRes – 2, VRes –
1 |