SNLS551B November 2017 – November 2018 DP83TC811R-Q1
PRODUCTION DATA.
The DP83TC811R-Q1 supports up to three configurable Light Emitting Diode (LED) pins: LED_0, LED_1, and LED_2 (CLKOUT). Several functions can be multiplexed onto the LEDs for different modes of operation. LED operations are selected using the LED_CFG1 Register 0x0460 – LED Configuration Register #1.
Because the LED output pins are also used as strap pins, external components required for strapping and the user must consider the LED usage to avoid contention. Specifically, when the LED outputs are used to drive LEDs directly, the active state of each output driver is dependent on the logic level sampled by the corresponding input upon power up or hardware reset.
Figure 28 shows the two proper ways of connecting LEDs directly to the DP83TC811R-Q1.