SLOS861C March 2015 – January 2023 DRV2700
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Understanding how the voltage driven onto a piezo actuator relates to the current consumption from the power supply is useful. Modeling a piezo element as a pure capacitor is reasonably accurate. Use Equation 4 to calculate the current through a capacitor for an applied sinusoid.
At the power supply, the actuator current is multiplied by the boost-supply ratio and divided by the efficiency of the boost converter as shown in Equation 5.
Substituting the design example values for the variables into Equation 5 and using a boost efficiency of 60%, yields a typical peak current from the power supply of 408 mA as shown in Equation 6.