SLVSFY8B February 2020 – August 2021 DRV8210
PRODUCTION DATA
The Absolute Maximum Ratings for the INx pins set the maximum voltage across the shunt resistor. If the signal on the INx pin is low, referenced at the board ground, then the INx pins are at a negative voltage with respect to the GND pin voltage. This sets the maximum sense voltage/GND pin voltage to 0.5 V. Figure 9-28 shows the relative pin voltages.
This example uses 150 mV for the maximum VSENSE, which is less than 0.5 V and provides some margin for safety or error. The maximum current through the motor will be the stall current, which is 1 A for this example. With this information, the sense resistance RSENSE can be calculated from the equation below.
Because the device GND pin voltage will vary with current through the sense resistor, the designers must also ensure that the logic pins meet VIL and VIH parameters,the MODE pin meets the VTIL, VTIZ, and VTIH parameters, and the supply remains above VUVLO for proper operation.