SLVSFY8B February 2020 – August 2021 DRV8210
PRODUCTION DATA
The figures below show waveform examples of high-side and low-side driving in half-bridge mode. Figure 9-15 and Figure 9-16 show example waveforms of driving a motor unidirectionally using high-side and low-side driving. Figure 9-17 and Figure 9-18 show example waveforms of driving a solenoid using high-side and low-side driving. Figure 9-19 and Figure 9-20 show examples of driving a motor using high-side and low-side driving when the OUTx pins are paralleled together to create a single half bridge.
Channel 1 = IN2 | Channel 2 = VOUT2 | Channel 4 = Motor Current |
Channel 1 = IN1 | Channel 2 = VOUT1 | Channel 4 = Solenoid Current |
Channel 1 = IN1, IN2 (paralleled) | Channel 2 = VVCC | Channel 3 = VOUT (OUT1/2 paralleled) |
Channel 8 = Motor Current |
Channel 1 = IN2 | Channel 2 = VOUT2 | Channel 4 = Motor Current |
Channel 1 = IN1 | Channel 2 = VOUT1 | Channel 4 = Solenoid Current |
Channel 1 = IN1, IN2 (paralleled) | Channel 5 = VVCC | Channel 6 = VOUT (OUT1/2 paralleled) |
Channel 8 = Motor Current |