SLVSD12D May 2015 – July 2019 DRV8305-Q1
PRODUCTION DATA.
The gate drive supply (VCP) of the DRV8305-Q1 is capable of delivering up to 30 mA (RMS) of current to the external power MOSFETs. The charge pump directly supplies the high-side N-channel MOSFETs and a 10-V LDO powered from VCP supplies the low-side N-channel MOSFETs. The designer can determine the approximate RMS load on the gate drive supply through the following equation.
Example: 36 nC (QG) × 6 (NSW) × 45 kHz (fSW) = 9.72 mA
Note that this is only a first-order approximation.