SNLS401C February 2012 – September 2018 DS90C187
PRODUCTION DATA.
The RFB pin determines the edge that the input LVCMOS data is latched on. If RFB is HIGH, input data is latched on the RISING EDGE of the pixel clock (IN_CLK). If RFB is LOW, the input data is latched on the FALLING EDGE of the pixel clock. Note: This can be set independently of receiver’s output clock strobe.
RFB | Result |
---|---|
0 | FALLING edge |
1 | RISING edge |