SPRS825F October 2012 – June 2020 F28M36H33B2 , F28M36H53B2 , F28M36P53C2 , F28M36P63C2
PRODUCTION DATA.
The C28x CPU is reset by the C28RSTIN signal, and the C28x CPU in turn resets the rest of the C28x Subsystem with the C28SYSRST signal. When reset, the C28x restarts program execution from the address provided at the top of the Boot ROM Vector Table.
The C28RSTIN has five possible sources: XRS, C28NMIWD, M3SWRST, M3DBGRST, and the M3RSNIN. The C28NMIWD is set in response to time-out conditions of the C28x NMI Watchdog. The M3SWRST is a software-generated reset output by the NVIC. The M3DBGRS is a debugger-generated reset that is also output by the NVIC. These two resets must be first enabled by the Cortex-M3 processor in order to propagate to the C28x Subsystem. M3RSNIN reset comes from the Cortex-M3 Subsystem to selectively reset the C28x Subsystem from Cortex-M3 software.
The C28x processor can learn the status of the internal ACIBRST reset signal and the external XRS pin by reading the DEVICECNF register.