SLLSFO4C December 2022 – September 2023 ISOM8710 , ISOM8711
PRODMIX
Table 9-1 lists the functional modes for the ISOM871x devices.
VCC STATE(2) | INPUT CURRENT IF(1) | OUTPUT | COMMENTS |
---|---|---|---|
PU | > ITH | L | Channel output assumes the inverse logic state of channel input. |
< ITH | H | ||
PD | X | Undetermined | When VCC is unpowered, the output is undetermined(2). When VCC transitions from unpowered to powered up, the channel output assumes the corresponding logic state based on the logic state of the input. |