8.1.1.1 RP_MAX
RP_MAX sets the upper limit of the LDC1001 resonant impedance input range.
- Configure the sensor such that the eddy current losses are minimized. As an example, for a proximity sensing application, set the distance between the sensor and the target to the maximum sensing distance.
- Measure the sensor impedance RP using an impedance analyzer.
- Multiply RP by 2 and use the next higher value from Table 7.
Setting RP_MAX to a value not listed in Table 7 can result in indeterminate behavior.