SNVSAY0 June 2017 LM317-N-MIL
PRODUCTION DATA.
Some layout guidelines must be followed to ensure proper regulation of the output voltage with minimum noise. Traces carrying the load current must be wide to reduce the amount of parasitic trace inductance and the feedback loop from VOUT to ADJ must be kept as short as possible. To improve PSRR, a bypass capacitor can be placed at the ADJ pin and must be located as close as possible to the IC. In cases when VIN shorts to ground, an external diode must be placed from VOUT to VIN to divert the surge current from the output capacitor and protect the IC. Similarly, in cases when a large bypass capacitor is placed at the ADJ pin and VOUT shorts to ground, an external diode must be placed from ADJ to VOUT to provide a path for the bypass capacitor to discharge. These diodes must be placed close to the corresponding IC pins to increase their effectiveness.
The LM317-N-MIL regulators have internal thermal shutdown to protect the device from over-heating. Under all operating conditions, the junction temperature of the LM317-N-MIL must not exceed the rated maximum junction temperature (TJ) of 125°C. A heatsink may be required depending on the maximum device power dissipation and the maximum ambient temperature of the application. To determine if a heatsink is needed, the power dissipated by the regulator, PD, must be calculate with Equation 3:
Figure 38 shows the voltage and currents which are present in the circuit.
The next parameter which must be calculated is the maximum allowable temperature rise, TR(MAX) in Equation 4:
where TJ(MAX) is the maximum allowable junction temperature (125°C for the LM317-N-MIL), and TA(MAX) is the maximum ambient temperature that will be encountered in the application.
Using the calculated values for TR(MAX) and PD, the maximum allowable value for the junction-to-ambient thermal resistance (θJA) can be calculated with Equation 5:
If the calculated maximum allowable thermal resistance is higher than the actual package rating, then no additional work is needed. If the calculated maximum allowable thermal resistance is lower than the actual package rating either the power dissipation (PD) needs to be reduced, the maximum ambient temperature TA(MAX) needs to be reduced, the thermal resistance (θJA) must be lowered by adding a heatsink, or some combination of these.
If a heatsink is needed, the value can be calculated from Equation 6:
where
When a value for θHA is found using the equation shown, a heatsink must be selected that has a value that is less than, or equal to, this number.
The θHA rating is specified numerically by the heatsink manufacturer in the catalog, or shown in a curve that plots temperature rise vs power dissipation for the heatsink.
The TO-263 (KTT), SOT-223 (DCY) and TO-252 (NDP) packages use a copper plane on the PCB and the PCB itself as a heatsink. To optimize the heat sinking ability of the plane and PCB, solder the tab of the package to the plane.
Figure 39 and Figure 40 show the information for the SOT-223 package. Figure 40 assumes a θJA of 74°C/W for 1-oz. copper and 59.6°C/W for 2-oz. copper and a maximum junction temperature of 125°C. See AN-1028 (SNVA036) for thermal enhancement techniques to be used with SOT-223 and TO-252 packages.
Figure 41 shows for the TO-263 the measured values of θJA for different copper area sizes using a typical PCB with 1-oz. copper and no solder mask over the copper area used for heatsinking.
As shown in Figure 41, increasing the copper area beyond 1 square inch produces very little improvement. It must also be observed that the minimum value of θJA for the TO-263 package mounted to a PCB is 32°C/W.
As a design aid, Figure 42 shows the maximum allowable power dissipation compared to ambient temperature for the TO-263 device (assuming θJA is 35°C/W and the maximum junction temperature is 125°C).
If the maximum allowable value for θJA is found to be ≥ 54°C/W (typical rated value) for the TO-252 package, no heatsink is needed because the package alone will dissipate enough heat to satisfy these requirements. If the calculated value for θJA falls below these limits, a heatsink is required.
As a design aid, Table 1 shows the value of the θJA of NDP the package for different heatsink area. The copper patterns that we used to measure these θJAs are shown in Figure 47. Figure 43 reflects the same test results as what are in Table 1.
Figure 44 shows the maximum allowable power dissipation versus ambient temperature for the TO-252 device. Figure 45 shows the maximum allowable power dissipation versus copper area (in2) for the TO-252 device. See AN-1028 (SNVA036) for thermal enhancement techniques to be used with SOT-223 and TO-252 packages.
LAYOUT | COPPER AREA | THERMAL RESISTANCE | |
---|---|---|---|
Top Side (in2)(1) | Bottom Side (in2) | (θJA°C/W) TO-252 | |
1 | 0.0123 | 0 | 103 |
2 | 0.066 | 0 | 87 |
3 | 0.3 | 0 | 60 |
4 | 0.53 | 0 | 54 |
5 | 0.76 | 0 | 52 |
6 | 1.0 | 0 | 47 |
7 | 0.066 | 0.2 | 84 |
8 | 0.066 | 0.4 | 70 |
9 | 0.066 | 0.6 | 63 |
10 | 0.066 | 0.8 | 57 |
11 | 0.066 | 1.0 | 57 |
12 | 0.066 | 0.066 | 89 |
13 | 0.175 | 0.175 | 72 |
14 | 0.284 | 0.284 | 61 |
15 | 0.392 | 0.392 | 55 |
16 | 0.5 | 0.5 | 53 |