SNVSCA9 October 2022 LM5012
PRODUCTION DATA
A Type 3 ripple generation network uses an RC filter consisting of RA and CA across SW and VOUT to generate a triangular ramp that is in phase with the inductor current. This triangular ramp is then AC-coupled into the feedback node using capacitor CB as shown in Figure 9-1. Type 3 ripple injection is suited for applications where low output voltage ripple is crucial.
Use Equation 16 and Equation 17to calculate RA and CA to provide the required ripple amplitude at the FB pin.
For the feedback resistor RFBT = 453 kΩ and RFBB = 49.9 kΩ values shown in Figure 9-1, Equation 16 dictates a minimum CA of 742 pF. In this design, a 3300-pF capacitance is chosen, which is done to keep RA within practical limits between 100 kΩ and 1 MΩ when using Equation 17.
Based on CA set at 3.3 nF, RA is calculated to be 226 kΩ to provide a 20-mV ripple voltage at FB. The general recommendation for a Type 3 network is to calculate RA and CA to get 20 mV of ripple at typical operating conditions. A smaller RA can need to be used to operate below nominal 48-V input. 12 mV of FB ripple or more must be ensured at the minimum input voltage of the design to ensure stability.
While the amplitude of the generated ripple does not affect the output voltage ripple, it impacts the output regulation as it reflects as a DC error of approximately half the amplitude of the generated ripple. For example, a converter circuit with Type 3 network that generates a 40-mV ripple voltage at the feedback node has approximately 10-mV worse load regulation scaled up through the FB divider to VOUT than the same circuit that generates a 20-mV ripple at FB. Use Equation 18 to calculate the coupling capacitance CB.
where
CB calculates to 56 pF based on a 75-µs settling time. This value avoids excessive coupling capacitor discharge by the feedback resistors during sleep intervals when operating at light loads. To avoid capacitance fall-off with DC bias, use a C0G or NP0 dielectric capacitor for CB.