SNVS532D October 2007 – August 2020 LM5067
PRODUCTION DATA
The configuration shown in Figure 9-6 requires three resistors (R1-R3) to set the thresholds.
The procedure to calculate the resistor values is as follows:
The resistors are calculated as follows:
The lower OVLO threshold is calculated from:
As an example, assume the application requires the following thresholds: VUVH = -36V, VUVL = -32V, VOVH = -60V.
The lower OVLO threshold calculates to -55.8V, and the OVLO hysteresis is 4.2V. Note that the OVLO hysteresis is always slightly greater than the UVLO hysteresis in this configuration.
When the R1-R3 resistor values are known, the threshold voltages and hysteresis are calculated from the following:
Ensure the voltages at the UVLO and OVLO pins do not exceed the Absolute Maximum ratings for those pins when the system voltage is at maximum.