SNVSC77A December 2024 – March 2025 LM5125-Q1
ADVANCE INFORMATION
Three main parameters are considered when selecting the inductance value: inductor current ripple ratio (RR), falling slope of the inductor current and the RHPZ frequency of the control loop.
According to peak current mode control theory, the slope of the slope compensation ramp must be greater than half of the sensed inductor current falling slope to prevent subharmonic oscillation at high duty cycle, that is:
where
The lower limit of the inductance can be found as:
Rcs is estimated to = 1.5mΩ, so the following can be found
The RHPZ frequency can be found as:
The crossover frequency must be lower than 1/5 of RHPZ frequency:
Assume a crossover frequency of 1kHz is desired, the upper limit of the inductance can be found as:
The inductor ripple current is typically set between 30% and 70% of the full load current, known as a good compromise between core loss and winding loss of the inductor.
Per phase input current can be calculated as:
In continuous conduction mode (CCM) operation, the maximum ripple ratio occurs at a duty cycle of 33%. The input voltage that result in a maximum ripple ratio can be found as:
Thus, the maximum input voltage Vin_max must be used to calculate the maximum ripple ratio.
For this example, a ripple ratio of 0.3, 30% of the input current was chosen. Knowing the switching frequency and the typical output voltage, the inductor value can be calculated as follows:
The closest standard value of 3.3μH was chosen for Lm.
The inductor ripple current at typical input voltage can be calculated as:
If a ferrite core inductor is selected, make sure the inductor does not saturate at peak current limit. The inductance of a ferrite core inductor is almost constant until saturation. Ferrite core has low core loss with a big size.
For powder core inductor, the inductance decreases slowly with increased DC current. This action leads to higher ripple current at high inductor current. For this example, the inductance drops to 70% at peak current limit compared to 0A. The current ripple at peak current limit can be found as: