SNVSBU4E June 2022 – August 2024 LM5177
PRODUCTION DATA
As soon as the on time in boost mode operation is lower then the minimum on time or the off time in buck mode is lower then the minimum off time, the control transits into the buck-boost operation. In the continuous current buck-boost mode, the control adds a boost magnetization (state I) switching cycle before the peak current is reached. Therefore, buck-boost operation mode always consists of all three switching cycles state I, state II, and state III. The peak current detection in this mode happens at the end of switching state I.