SNVSCH2 September 2024 LM65645-Q1
ADVANCE INFORMATION
this example uses the fixed output voltage mode to set the output voltage to 5V, by connecting the FB pin to the VCC pin.
If an output voltage different from either 3.3V or 5V is required, then the adjustable output voltage mode must be used. In that case, an external voltage divider must be connected between the output node and the FB pin, while Equation 5 and Equation 6 are used to determine the divider values.
Note that Equation 6 states that the parallel combination of RFBB and RFBT must be greater than 4kΩ and less than 100kΩ. This limit is required because the regulator must reliably detect the sate of the FB pin during the start-up sequence to set the output voltage mode correctly.
If the adjustable output voltage mode was chosen for this example, then values of RFBT = 100kΩ and RFBB = 19.1kΩ satisfy both Equation 5 and Equation 6.
For more details, see Section 7.3.1.