SNAS744B July 2017 – March 2018 LMS3655
PRODUCTION DATA.
The LMS3655 is designed to have very low input supply current when regulating light loads. This is achieved by powering much of the internal circuitry from the output. The BIAS pin is the input to the LDO that powers the majority of the control circuits. By connecting the BIAS input to the output of the regulator, this current acts as a small load on the output. This current is reduced by the ratio of VOUT / VIN, just like any other load.
IQ_VIN is defined as the current consumed by a converter using a LMS3655 device while regulating without a load. To calculate the theoretical total quiescent current, the below equation can be used with parameters from the Electrical Characteristics and System Characteristics tables. While operating without a load, the LMS3655 only powers itself. The device draws power from three sources: the VIN pin (IQ), the EN pin (IEN), and the BIAS pin (IB). Because the BIAS input is connected to the output of the circuit, the power consumed is converted from input power with an effective efficiency, ηeff. Here, effective efficiency is the added input power needed when lightly loading the converter of the LMS3655 device and is divided by the corresponding additional load. This allows unloaded current to be calculated in Equation 2:
where
NOTE
The EN pin consumes a few micro-amperes when tied to high; see IEN. Add IEN to IQ as shown in Equation 2 if EN is tied to VIN. If EN is tied to a voltage less than 5 V, virtually no current is consumed allowing EN to be used as an UVLO pin once a voltage divider is added.