SNVSCD0C November 2023 – December 2024 LP5810
PRODUCTION DATA
After VCC powering up, the device can be initialized by configuring chip_en = 1 after executing I2C slave addressing. Then the CONFIG registers can be set to the excepted configuration. After updating the CONFIG registers, one update command must to be sent to make the configuration effective. Either manual mode or autonomous mode can be seleted for each LED. A new configuration is only effective once update command is received.
The detailed program procedure is illustrated as: