SLVSGD5 July 2021 LP5890
PRODUCTION DATA
The continuous Clock Series Interface (CCSI) provides access to the programmable functions and registers, SRAM data of the device. The interface contains two input digital pins. The pins are the serial data input (SIN) and serial clock (SCLK). Moreover, there is an another wire called serial data output (SOUT) as the output digital signal of the device. The SIN is set to HIGH when device is in idle status and the SCLK needs to be existent and continuous all the time considering it is the clock source of internal Frequency Multiplier. The SOUT is used to transmit the data or read the data of internal registers.
This protocol can support up to 32 devices cascaded in a data chain. The devices will receive the chip index command after power up. The chip index command will configure addresses of the devices from 0x00 up to 0x1F according to the sequence that receives the command. Then the controller can communicate with all the devices through the broadcast way or particular device through non-broadcast way.
The broadcast is mainly used to transmit function control commands. All the devices in a data chain will receive the same data in this way. The non-broadcast is mainly used to transmit function control commands or display data, and each device receives its own data in this way. These two ways are distinguished by the command identification.