SLDS269A March 2022 – May 2022 LP5891
PRODUCTION DATA
Figure 7-1 shows an implementation of a 16 × 32 RGB LED matrix using two LP5891 devices in independent mode. Each device is responsible for its own 16 ×16 RGB LED matrix, which means that all the data for section A is stored in device 1 and the data for section B is stored in device 2.
The unused line must be assigned to the last several lines of the device. For example, if there are only 14 scanning lines, then the two unused lines must be assigned to 1_LS14 and 1_LS15.