SLVSHF3 October 2024 LP5899-Q1
PRODUCTION DATA
The LP5899-Q1 only requires two external components. Place the capacitor for the VCC input as close as possible to the VCC pin. The FAULT pin is an open drain output. When the FAULT pin is connected to the Controller, an external pull-up resistor is required.