SLVSHF3 October 2024 LP5899-Q1
PRODUCTION DATA
The data on SDI wire must be stable at the rising edge of the SCLK wire. The data on SDO shifts out at the falling edge of the SCLK wire. SDO can be forced to be disabled by the bit SPI_SDO_DIS in the SPICTRL register. This is useful when the same command is broadcasted to multiple LP5899-Q1 devices on a single SPI bus. When no data is shifted into the device, the SCLK wire is expected to be logic LOW.