SDLS975 April 2024 LSF0002
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
To enable the I/O pins, the VBIAS input should be referenced towards the lower power supply (in the following example, VEXT,A) during voltage translation. To be in the high impedance state during power-up, power-down, or during operation, the VBIAS pin must be pulled low and at GND or disabled by an open-drain driver without a pullup resistor. Use the VBIAS pin to properly bias the I/O channels. A filter capacitor on VBIAS is also recommended for a stable supply at the device.
The supply voltage of open drain I/O devices can be completely different from the supplies used for the LSF and has no impact on the operation. For additional details on how to use the enable pin, see the Using the Enable Pin with the LSF Family video.
INPUT VBIASPIN | Data Port State |
---|---|
Tied directly to VBIAS | An = Bn |
L | Hi-Z |