Forward-Reverse speed profiles can be configured
by setting SPEED_PROFILE_CONFIG to b11. Forward-Reverse speed profiles feature
direction change through adjusting the duty command. DUTY_C configures duty command
at which the direction will be changed. The Forward-Reverse speed profile can be
used to eliminate the separate signal used to control the motor direction.
- DUTY_ON1 configures the duty command above which MCF8316A starts driving the
motor in the forward direction (to speed reference set by SPEED_CLAMP1) when
the current speed reference is zero. When current speed reference is zero
and duty command is below DUTY_ON1, MCF8316A continues to be in off state
and motor is stationary.
- DUTY_OFF1 configures the duty command below which
the speed reference changes in the forward direction from SPEED_CLAMP1 to
SPEED_OFF1, if SPEED_OFF1 > SPEED_CLAMP1. If SPEED_OFF1 < SPEED_CLAMP1,
speed reference is set to SPEED_CLAMP1.
- DUTY_CLAMP1 configures the duty command at which
speed reference will be the constant in forward direction. SPEED_CLAMP1
configures constant speed reference between DUTY_CLAMP1 and DUTY_OFF1.
- DUTY_A configures the duty command for speed
reference SPEED_A. The speed reference changes linearly between DUTY_CLAMP1
and DUTY_A.
- DUTY_B configures the duty command above which
MCF8316A will be in off state. The speed reference remains constant at
SPEED_A between DUTY_A and DUTY_B.
- DUTY_C configures the duty command at which the
direction is changed
- DUTY_D configures the duty command above which
the MCF8316A will be in running state in the reverse direction. SPEED_D
configures constant speed reference between DUTY_D and DUTY_E.
- DUTY_CLAMP2 configures the duty command above
which speed reference will be constant at SPEED_CLAMP2 in reverse direction.
The speed reference changes linearly between DUTY_E and DUTY_CLAMP2.
- DUTY_ON2 configures the duty command below which MCF8316A starts driving the
motor in the reverse direction (to speed reference set by SPEED_CLAMP2) when
the current speed reference is zero. When current speed reference is zero
and duty command is above DUTY_ON1, MCF8316A continues to be in off state
and motor is stationary.
- DUTY_OFF2 configures the duty command above which the speed reference
changes in the reverse direction from SPEED_CLAMP2 to SPEED_OFF2.