SBOS382H may 2008 – june 2023 OPA2673
PRODUCTION DATA
The OPA2673 is built using a high-speed complementary bipolar process. The internal junction breakdown voltages are shown in the Absolute Maximum Ratings. All device pins have limited ESD protection using internal diodes to the power supplies, as shown in Figure 9-5.
These diodes provide moderate protection to input overdrive voltages above the supplies as well. The protection diodes typically support a 10‑mA continuous current. Where higher currents are possible (for example, in systems with ±15‑V supply parts driving into the OPA2673), add current-limiting series resistors into the two inputs.