SBOS309E August 2004 – December 2024 OPA2830
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The OPA2830 is a unity-gain stable, voltage-feedback op amp; therefore, a wide range of resistor values can be used for the feedback and gain setting resistors. The primary limits on these values are set by dynamic range (noise and distortion) and parasitic capacitance considerations. For a noninverting unity-gain follower application, the feedback connection can be made with a direct short.
Less than 200Ω, the feedback network presents additional output loading that can degrade the harmonic distortion performance of the OPA2830. Greater than 1kΩ, the typical parasitic capacitance (approximately 0.2pF) across the feedback resistor can cause unintentional band limiting in the amplifier response.
Recommended to target the parallel combination of RF and RG (see Figure 8-3) to be less than about 400Ω. The combined impedance RF || RG interacts with the inverting input capacitance, placing an additional pole in the feedback network, and thus a zero in the forward response. Assuming a 2pF total parasitic on the inverting node, holding RF || RG < 400Ω keeps the pole above 200MHz. This constraint implies that the feedback resistor RF can increase to several kΩ at high gains. This is acceptable as long as the pole formed by RF and any parasitic capacitance appearing in parallel is kept out of the frequency range of interest.
In the inverting configuration, an additional design consideration must be noted. RG becomes the input resistor and therefore the load impedance to the driving source. If impedance matching is desired, RG can be set equal to the required termination value. However, at low inverting gains, the resultant feedback resistor value can present a significant load to the amplifier output. For example, an inverting gain of 2 with a 50Ω input matching resistor (= RG) requires a 100Ω feedback resistor, which contributes to output loading in parallel with the external load. In such a case, preferably to increase both the RF and RG values, and then achieve the input matching impedance with a third resistor to ground (see Figure 8-15). The total input impedance becomes the parallel combination of RG and the additional shunt resistor.