SBOS771B December 2016 – November 2024 OPA4277-SP
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The OPA4277-SP operates from ±2-V to ±18-V supplies with excellent performance. Unlike most operational amplifiers that are specified at only one supply voltage, the OPA4277-SP precision operational amplifier is specified for real-world applications; a single limit applies over the ±5-V to ±15-V supply range. High performance is maintained as the amplifier swings to the specified limits. Because the initial offset voltage is so low (±50-µV, max), user adjustment is usually not required.