SLTS278J November 2010 – March 2020 PTH08T250W
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
When using TurboTrans while paralleling two modules, the TurboTrans resistor, RTT, must be connected from the TurboTrans pin (pin 19) of the Master module to the +Sense pin (pin 17) of the Master module. When paralleling modules the procedure to calculate the proper value of output capacitance and RTT is similar to that explained in the section, however the values must be calculated for a single module. Therefore, the total output current load step must be halved before determining the required output capacitance and the RTT value as explained in the section. The value of output capacitance calculated is the minimum required output capacitance per module and the value of RTT must be calculated using this value of output capacitance. The TurboTrans pin of the Slave module must be left open.
As an example, take a look at a 12-V application requiring a 60 mV deviation during an 30 A load transient. A majority of 470 μF, 10 mΩ output capacitors are used. Use the 12 V, Type B capacitor chart, Figure 15. First, halving the load transient gives 15 A. Dividing 60 mV by 15 A gives 4 mV/A transient voltage deviation per amp of transient load step. Select 4 mV/A on the Y-axis and read across to the 'With TurboTrans' plot. Following this point down to the X-axis gives us a minimum required output capacitance of approximately 1500 μF. This is the minimum required output capacitance per module. Hence, the total minimum output capacitance is 2 × 1500 μF = 3000 μF. The required RTT resistor value for 1500 μF can then be calculated or selected from Table 5. The required RTT resistor is approximately 17.4 kΩ.