SLASEH7H October 2019 – January 2023 TAS5825M
PRODUCTION DATA
The DVDD supply that is required from the system is used to power several portions of the device. As shown in Figure 10-12, the DVDD supply provides power to the DVDD pin. Proper connection, routing and decoupling techniques are highlighted in Section 10 and Section 10.4.2 and must be followed as closely as possible for proper operation and performance.
Some portions of the device also require a separate power supply that is a lower voltage than the DVDD supply. To simplify the power supply requirements for the system, the TAS5825M device includes an integrated low dropout (LDO) linear regulator to create this supply. This linear regulator is internally connected to the DVDD supply and the output is presented on the DVDD_REG pin, providing a connection point for an external bypass capacitor. Note that the linear regulator integrated in the device has only been designed to support the current requirements of the internal circuitry, and must not be used to power any additional external circuity. Additional loading on this pin can cause the voltage to sag, negatively affecting the performance and operation of the device.