SLOSE88 December 2024 TAS6754-Q1
ADVANCE INFORMATION
The device monitors temperature with five temperature sensors. Every output channel has a temperature sensor in close proximity to the center of its output stage to monitor the temperature of each channel separately. An additional temperature sensor is located in a global position on the die, so it better represents the actual die junction temperature. Based on these sensors, warning and fault signals can be generated. A Thermal Gain Foldback scheme is available that autonomously regulates audio gain and consequently limits die temperature.