SBOS831B December 2016 – June 2021 THS4552
PRODUCTION DATA
The most important elements to the closed-loop performance are the open-loop gain and open-loop output impedance. Figure 8-1 and Figure 8-2 show the simulated differential open-loop gain and phase from the differential inputs to the differential outputs with no load and with a 100 Ω load. Operating with no load removes any effect introduced by the open-loop output impedance to a finite load. This AOL simulation removes the 0.6 pF internal feedback capacitors to isolate the forward path gain and phase (see Figure 12-1). The 0.6 pF capacitance becomes part of the feedback network that sets the noise gain and phase combined with the external elements. The simulated differential open-loop output impedance is shown in Figure 8-3.
This impedance combines with the load to shift the apparent open-loop gain and phase to the output pins when the load changes. The rail-to-rail output stage shows a very high impedance at low frequencies that reduces with frequency to a lower midrange value and then peaks again at higher frequencies. The maximum value at low frequencies is set by the common-mode sensing resistors to be a 10.5 kΩ dc value (see Section 8.2). This high impedance at a low frequency is significantly reduced in closed-loop operation by the loop gain, as shown in the closed-loop output impedance of Figure 6-38. Figure 8-1 compares the no load AOL gain to the AOL gain driving a 100 Ω load that shows the effect of the output impedance. The heavier loads pull the AOL gain down faster to lower crossovers with more phase shift at the lower frequencies.
The much faster phase roll-off for the 100 Ω differential load explains the greater peaked response illustrated in Figure 6-4 and Figure 6-22 when the load decreases. This same effect happens for the RC loads common with converter interface designs. Use the TINA-TI™ model to verify loop phase margin in any design.