SLVS238L August 1999 – November 2024 TL331 , TL331B , TL391B
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Output current is determined by the load/pull-up resistance and logic/pull-up voltage. The output current produces a output low voltage (VOL) from the comparator. In which VOL is proportional to the output current. Use Output Low Voltage vs Output Current (IOL) to determine VOL based on the output current.
The output current can also effect the transient response. More is explained in the next section.