SLVS029H January 1984 – November 2015 TL499A
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
One or two power sources will be regulated to an output voltage set by two feedback resistors.
Figure 3 shows the basic configuration of the two power source voltage regulator
Provide one or more of the following power sources:
Select RCL value based on Table 1 through Table 5.
OUTPUT VOLTAGE (V) | SWITCHING REGULATOR INPUT VOLTAGE (SW REG IN2) (V) | ||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
1.1 | 1.2 | 1.3 | 1.5 | 1.7 | 2 | 2.5 | 3 | 5 | 6 | 9 | |||
OUTPUT CURRENT (mA) | |||||||||||||
30 | 65 | 90 | |||||||||||
25 | 50 | 80 | 100 | ||||||||||
20 | 20 | 25 | 30 | 85 | 100 | 100 | |||||||
15 | 15 | 20 | 30 | 45 | 55 | 100 | 100 | 100 | |||||
12 | 10 | 15 | 20 | 25 | 30 | 40 | 55 | 70 | 100 | 100 | 100 | ||
10 | 15 | 20 | 25 | 30 | 35 | 45 | 65 | 80 | 100 | 100 | |||
9 | 20 | 25 | 25 | 35 | 40 | 50 | 70 | 90 | 100 | 100 | |||
6 | 30 | 35 | 40 | 45 | 55 | 75 | 95 | 100 | |||||
5 | 35 | 40 | 45 | 55 | 70 | 85 | 100 | 100 | Circuit of Figure 1, except: RCL = 150 Ω CF = 330 μF CP = 0.1 μF |
||||
4.5 | 35 | 45 | 50 | 60 | 75 | 95 | 100 | 100(1) | |||||
3 | 55 | 65(1) | 75(1) | 95(1) | 100(1) | ||||||||
2.9 | 60(1) | 70(1) | 75(1) | 100(1) | 100(1) |
OUTPUT VOLTAGE (V) | SWITCHING REGULATOR INPUT VOLTAGE (SW REG IN2) (V) | ||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
1.1 | 1.2 | 1.3 | 1.5 | 1.7 | 2 | 2.5 | 3 | 5 | 6 | 9 | |||
OUTPUT CURRENT (mA) | |||||||||||||
30 | 50 | 100 | |||||||||||
25 | 50 | 70 | 100 | ||||||||||
20 | 15 | 25 | 30 | 70 | 90 | 100 | |||||||
15 | 10 | 15 | 25 | 35 | 45 | 90 | 100 | 100 | |||||
12 | 10 | 10 | 15 | 20 | 25 | 35 | 45 | 60 | 100 | 100 | 100 | ||
10 | 15 | 20 | 20 | 25 | 30 | 40 | 55 | 70 | 100 | 100 | |||
9 | 20 | 20 | 25 | 30 | 35 | 45 | 60 | 80 | 100 | ||||
6 | 25 | 30 | 35 | 45 | 50 | 65 | 90 | 100 | |||||
5 | 30 | 35 | 40 | 55 | 60 | 75 | 100 | 100 | Circuit of Figure 1, except: RCL = 200 Ω CF = 330 μF CP = 0.1 μF |
||||
4.5 | 35 | 40 | 45 | 55 | 65 | 85 | 100 | 100(1) | |||||
3 | 50 | 55(1) | 65(1) | 80(1) | 90(1) | ||||||||
2.9 | 50(1) | 60(1) | 65(1) | 85(1) | 100(1) |
OUTPUT VOLTAGE (V) | SWITCHING REGULATOR INPUT VOLTAGE (SW REG IN2) (V) | ||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
1.1 | 1.2 | 1.3 | 1.5 | 1.7 | 2 | 2.5 | 3 | 5 | 6 | 9 | |||
OUTPUT CURRENT (mA) | |||||||||||||
30 | 40 | 70 | |||||||||||
25 | 40 | 55 | 100 | ||||||||||
20 | 10 | 15 | 20 | 55 | 70 | 100 | |||||||
15 | 10 | 10 | 20 | 30 | 35 | 75 | 95 | 100 | |||||
12 | 10 | 10 | 10 | 15 | 20 | 25 | 35 | 45 | 95 | 100 | 100 | ||
10 | 15 | 15 | 15 | 20 | 25 | 30 | 45 | 55 | 100 | 100 | |||
9 | 15 | 15 | 20 | 25 | 30 | 35 | 50 | 60 | 100 | 100 | |||
6 | 25 | 25 | 30 | 35 | 45 | 55 | 70 | 90 | |||||
5 | 30 | 30 | 35 | 45 | 50 | 65 | 85 | 100 | Circuit of Figure 1, except: RCL = 300 Ω CF = 330 μF CP = 0.1 μF |
||||
4.5 | 30 | 35 | 40 | 45 | 55 | 70 | 95 | 100(1) | |||||
3 | 45 | 50(1) | 55(1) | 70(1) | 90(1) | ||||||||
2.9 | 45(1) | 50(1) | 60(1) | 75(1) | 95(1) |
OUTPUT VOLTAGE (V) | SWITCHING REGULATOR INPUT VOLTAGE (SW REG IN2) (V) | ||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
1.1 | 1.2 | 1.3 | 1.5 | 1.7 | 2 | 2.5 | 3 | 5 | 6 | 9 | |||
OUTPUT CURRENT (mA) | |||||||||||||
30 | 30 | 50 | |||||||||||
25 | 25 | 40 | 75 | ||||||||||
20 | 40 | 55 | 90 | ||||||||||
15 | 15 | 20 | 55 | 70 | 100 | ||||||||
12 | 10 | 15 | 25 | 35 | 65 | 80 | 100 | ||||||
10 | 10 | 20 | 25 | 30 | 40 | 70 | 85 | ||||||
9 | 10 | 10 | 10 | 15 | 20 | 25 | 35 | 45 | 75 | 100 | |||
6 | 15 | 20 | 20 | 25 | 30 | 35 | 50 | 60 | |||||
5 | 20 | 20 | 35 | 30 | 35 | 45 | 55 | 70 | Circuit of Figure 1, except: RCL = 510 Ω CF = 330 μF CP = 0.1 μF |
||||
4.5 | 25 | 25 | 30 | 35 | 40 | 50 | 65 | 90(1) | |||||
3 | 35 | 35(1) | 40(1) | 50(1) | 75(1) | ||||||||
2.9 | 35(1) | 35(1) | 40(1) | 55(1) | 80(1) |
OUTPUT VOLTAGE (V) | SWITCHING REGULATOR INPUT VOLTAGE (SW REG IN2) (V) | ||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
1.1 | 1.2 | 1.3 | 1.5 | 1.7 | 2 | 2.5 | 3 | 5 | 6 | 9 | |||
OUTPUT CURRENT (mA) | |||||||||||||
30 | 35 | ||||||||||||
25 | 35 | 50 | |||||||||||
20 | 35 | 60 | |||||||||||
15 | 10 | 30 | 45 | 65 | |||||||||
12 | 20 | 40 | 45 | 85 | |||||||||
10 | 15 | 25 | 40 | 55 | |||||||||
9 | 10 | 10 | 15 | 25 | 30 | 45 | 60 | ||||||
6 | 10 | 10 | 10 | 15 | 20 | 20 | 30 | 35 | |||||
5 | 10 | 10 | 15 | 20 | 20 | 25 | 35 | 40 | Circuit of Figure 1, except: RCL = 1 kΩ CF = 330 μF CP = 0.1 μF |
||||
4.5 | 15 | 15 | 15 | 20 | 25 | 30 | 40 | 45(1) | |||||
3 | 20 | 25(1) | 25(1) | 30(1) | 35(1) | ||||||||
2.9 | 20(1) | 25(1) | 25(1) | 30(1) | 45(1) |
Select the values for RE1and RE2 using Equation 1:
IOUT = 50 mA |