SLVSG10D November 2021 – July 2022 TLC6984
PRODUCTION DATA
The TLC6984 can operate in two different modes: independent or stackable. In independent mode, a single TLC6984 can drive a 16 × 16 RGB LED matrix, while in stackable mode, up to four TLC6984s can be stacked together, which means the line switches of one device can be shared to the others. Stacking three TLC6984s can drive a 48 × 48 RGB LED matrix while stacking four TLC6984s can drive a 64 × 64 RGB matrix. The mode can be configured by the MOD_SIZE (see FC2 for more details).