SBOS817I June 2017 – August 2021 TLV6741 , TLV6742
PRODUCTION DATA
The transfer function defining the relationship between VOUT and the AC input signal is shown in Equation 1:
The required gain can be calculated based on the expected input signal level and desired output level as shown in Equation 2:
Select a standard 10-kΩ feedback resistor and calculate RG.
To minimize the attenuation in the desired passband from 300 Hz to 3 kHz, set the upper (fH) and lower (fL) cutoff frequencies outside of the desired bandwidth as:
and
Select CG to set the fL cutoff frequency using Equation 6:
Select CF to set the fH cutoff frequency using Equation 7:
The input signal cutoff frequency should be set low enough such that low-frequency sound waves still pass through. Therefore select CIN to achieve a 30-Hz cutoff frequency (fIN) using Equation 8:
The measured transfer function for the microphone preamplifier circuit is shown in Figure 9-2 and the measured THD+N performance of the microphone preamplifier circuit is shown in Figure 9-3.