SLYS056 August 2024 TMAG5233
ADVANCE INFORMATION
The TMAG5233 SOT-23 detects the magnetic flux density which is horizontal to the package marking surface.
Magnetic flux density traveling from the pin 2 side of the package to the pin 1 side of the package is considered positive, while magnetic flux density traveling from the pin 1 side of the package to the pin 2 side of the package is considered negative.
A magnet creates a three-dimensional magnetic field that permeates the surrounding space, with field strength and direction varying at different points. This variation allows for multiple ways to induce a positive (or negative) magnetic flux density, as illustrated in Figure 7-4 and Figure 7-5.